Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Daisy chain multiple VL53l1X - lack of information about GPIO1

Hello,due to the bad datasheet and missing register map it is almost impossible to get information about GPIO1. The only settings i found are affecting the interrupt functionality. But why is the pin called GPIO when only used as interrupt output. Sh...

MStoc.1 by Associate
  • 1254 Views
  • 2 replies
  • 0 kudos

Prefered colour surface background for outdoors (VL6180X)

Hello,I am experimenting some trouble when using sensor VL6180X outdoors due to sunlight.The lasers are continuously seeing a yellow surface at 15cm. I get good rangings under Indoor light condition.The point is the lasers do not see any backgound w...

Jhern.1 by Associate II
  • 2340 Views
  • 4 replies
  • 0 kudos

Reliability for VL53L0CX

Hello, I'm using VL53L0CXV0DH/1 within the construction of a more global solution and would like to have information about its reliability.Can you please help provide reliability information like Failure rate, Lifetime, MTBF, Warranty for the product...

GDjam.1 by Associate
  • 1462 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L3CX XSHUT PIN PROBLEM IN DEEP SLEEP

I have project using a VL53L3CX distance sensor. Also , I control it by ESP32. In normally, I can command to XSHUT pin. And I can read xshut pin of ESP32 that is 3V3 or 0V.But, When ESP32 enters deep-sleep mode for current consumption, XSHUT pin of t...

0693W00000Lyp5aQAB.png 0693W00000Lyp5VQAR.png
fafeyto by Associate II
  • 1690 Views
  • 1 replies
  • 0 kudos

VL53L0X_GetInterruptMaskStatus fails

We are trying to get a VL53L0X sensor to run but VL53L0X_GetInterruptMaskStatus() constantly fails and we cant perform any measurements. We compiled the API provided by ST provided from https://www.st.com/en/imaging-and-photonics-solutions/vl53l0x.ht...

MMeng.3 by Associate II
  • 1368 Views
  • 1 replies
  • 0 kudos