2022-04-04 8:53 AM
Hi,
I have some questions about the VL53L5CX maximum range. I am trying to reliably detect an oxygen cylinder passing through a portal 1200mm by 2133mm (floor level). The sensor is mounted at the top of the portal. I can detect cylinder up to approx. 1500mm with the following test conditions but need 2000mm.
According to the VL53L5CX datasheet, the sensor has a max range of 4000mm but drops to 1000mm under my design conditions.
Is detection of the oxygen cylinder at 2000mm a realistic number for this design?
Can sensor driver firmware be tweaked to increase motion detection range with a reduction of distance accuracy to achieve 2000mm.
Mark
2022-04-04 9:39 AM
The ability to range depends on target size and target reflectivity. That 4M is obtained by ranging on a large white wall. It's basically the absolute max. (Or the number we guarantee you cannot exceed.)
A target of 100mm dia and 20% reflectivity is not much of a target. I fully agree that max range of 1M would be an expected result.
There are really only a few things you can do to turn an undetectable target into a detectable target.
Get larger, get closer, or get brighter.
In your case, brighter seems to the be the only easy choice.
A bit of retro-reflective tape would do it. It doesn't even have to be a very large bit to make a large difference.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.