Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Lowering power consumption

Hi,I am currently implementing an application using VL53L1X sensor with NRF52. Our applicaiton needs to consume very low current in order to get long battery life. I am reading VL53L1X sensor data every minute. While i am not reading any VL53L1X data...

TGund by Associate
  • 2450 Views
  • 4 replies
  • 0 kudos

Estmated max size of parameters

I'm referencing to STSW-IMG009 and specifically function VL53L1X_SetInterMeasurementInMs(uint32_t InterMeasMs)What would be the maximum size of the argument and the value of ClockPLL. I'm re-writing for another platform.Regards/Claes

Ckjel.1 by Associate
  • 1032 Views
  • 1 replies
  • 0 kudos

[Proximity Sensor ADC with DMA Problem] I have GP2Y0A41SK0F Sharp for distance measuring sensor. the datasheet says it needs 16.5 ms with 3.7 ms tolerant. for sampling time. So I assumed I need to configure PCLK2 (I use ADC2), ADC Clock Prescaller, ...

channel sampling, then calculate those parameters until 16.5 ms found. The problem is kinda impossible to get 16.5 ms even I tried to adjust those parameter. anyone has a clue? Iam using STM32F407VGx

I get the same histogram data every time on VL53l3cx

As shown below, the first line is the distance and the rest are histogram data whci I think is same and not correct?103-4652409,-2097499426,1344930034,1327221713,525211626,33064954,-17059034,235676156,1093868795,138478570,-1947005701,2044266306,-9799...

DMehr.2 by Associate II
  • 1297 Views
  • 2 replies
  • 0 kudos

Where can I find the i2c registers for the VL53L3CX? I am trying to implement this in a design with an FPGA, but I cannot find any information regarding the registers in the datasheet.

Where can I find the i2c registers for the VL53L3CX? I am trying to implement this in a design with an FPGA, but I cannot find any information regarding the registers in the datasheet.We are looking at simply taking a range measurement every time the...

PFlet.1 by Associate
  • 1003 Views
  • 1 replies
  • 0 kudos

How to use VL53L3CX with STM32WLE5JC ??!

I own a small dev board (LoRa-E5 mini from SeeedStudio) and coding using STM32cube IDE + MX.I have made project from scratch, using LED, switch, UART (works fine !)... and now I want to use my VL53L3CX-SATEL board.The board is defined on I2C2, all lo...

SC26 by Associate II
  • 2828 Views
  • 6 replies
  • 0 kudos

VL53L5CX Register description

I just started working with VL53L5CX but can't find details on the commands/registers. I had a look to the example code and can use it but I can only guess what the different settings send via i2c to the firmware will do. I also studied the different...

PBoer.1 by Associate II
  • 2262 Views
  • 3 replies
  • 0 kudos