2022-05-16 1:59 AM
Hello,
due to the bad datasheet and missing register map it is almost impossible to get information about GPIO1. The only settings i found are affecting the interrupt functionality. But why is the pin called GPIO when only used as interrupt output. Shouldn't it be called INT? Is it possible to use it to daisy chain multiple sensors? Sensor 1 GPIO1 => Sensor 2 XShut, Sensor 2 GPIO => Sensor 3 Xshut...
Thanks, Manuel
2022-05-16 2:08 AM
Hello,
It is called indeed GPIO by the HW but used as an INT by the FW. So, you can not daisy chain multiple sensors. Sorry about that,
Anne
2022-05-16 4:06 AM
Hi Anne,
thanks for you reply.
But didn't your engineers thougth about using multiple sensors?
It could be so easy with a daisy chain.
Enable first sensor, set address, enable next sensor, set address...
Only 5 wires would be used for all sensors.
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.