Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L3 Emitter Exclusion (Angle)Cone Problem

Hi everyone,I have problem for VL53L3CXV0DH/1. It is very difficult to describe the problem. I hope I can explain. You know that angles of VL53L3CXV0DH is like below.I have PCB that includes VL53L3. The light will flash each time if the sensor detect...

0693W00000NqKe2QAF.png 0693W00000NqKn4QAF.png 0693W00000NqKniQAF.png 0693W00000NqKo7QAF.png
fafeyto by Associate II
  • 1747 Views
  • 1 replies
  • 0 kudos

about GUI installation for X-NUCLEO-53L1A1

We bought P-NUCLEO-53L1A1 for testing the performance of VL53L1X.We met some trouble for setup and software installation.According to the Quick Start Guide for X-NUCLEO-53L1A1), we tried toinstall VL53L1X GUI to our PC, but failed. Attached images f...

DSai.1 by Associate III
  • 1159 Views
  • 2 replies
  • 0 kudos

Resolved! vl53l1x shortest distance measurement

I have a vl53l1x and testing it without glass and uncalibrated operating in SHORT distance mode. I get distance measurements of non-zero values at about 120mm. The datasheet claims 4cm. Will the calibration process result in short measurements inline...

WMaho.1 by Associate
  • 1604 Views
  • 1 replies
  • 0 kudos

VL53L5CX - Several sensors in parallel

I worked with a single VL53L5CX under Linux without problems. Now I wan't to have at least two sensors running in parallel connected to the same I2C bus. So I followed the documentation and first set LPn for the sensor which should keep its address (...

PBoer.1 by Associate II
  • 1479 Views
  • 1 replies
  • 0 kudos