2020-07-13 2:48 AM
I made a PCB using Teseo-LIV3F as stand alone, tried to connect TX and RX of the module to Arduino TX and RX using I TinyGps++ library, but I couldn't get any response from the module. I tried to connect the module to software and hardware serial of the Arduino and couldn't also get any response. When I connect the module to USB to TTL I could get response. I am using an active antenna. I have attached the schematic which I am using. Hope to get some help to solve my problem.
Best regards
Solved! Go to Solution.
2020-07-16 6:33 AM
Hi
Your schematic make sense
You are using tps22093 to provide power to the antenna... voltage comes from VCCRF (correct) and ANT_OFF to enable/disable the switch. This parts can not impact LIV working.... at least (in Over current) it could turnoff the antenna no more than that.
I don't understand where VCC power comes from. I see VIN is the same for LIV and TPS781... but who is providing VIN?
2020-07-13 2:53 AM
Hi
Do you see the PPS pulsing?
Is LIV3F out-of-Reset (Reset pins has to be high to guarantee LIV running)
Regards
Francesco
2020-07-13 3:03 AM
Hi, I have no pin out for PPS and Reset pins to the Arduino. I don't understand why when i connect the TX,RX OF Teseo to USB to TTL I could see that the module responses. The pins PPS and Reset in my schematic that i share with you are have no pinout to th MCU.
2020-07-13 3:06 AM
I just can see NEMA information when I connect USB to TTL
2020-07-13 3:13 AM
Which values do you have on:
2020-07-13 3:29 AM
3.3v
2020-07-13 3:54 AM
Is the schematic correct? Is there any need to connect PPS and rest to the MCU?
2020-07-13 10:06 AM
Perhaps you have the RX/TX sense backward on the Arduino, or the baud rate is wrong.
2020-07-14 7:27 AM
Schematic seems correct
PPS and Reset pins can stay not-connected (LIV has internal resistor to guarantee correct value)
Voltage 3.3 is OK
It has to be running
Just for testing could you add a LED on the PPS? just to understand if LIV is running.
2020-07-15 1:04 AM
Thanks for help, I will try that. I also measure the TPS out pin and it was 1.2V, even i can see the vcc Rf is 3.3v, is that normal?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.