2021-07-23 11:34 AM
Hello. I've developed the board based on TESEO LIV3R module. I have successfully developed and debug code on X-NUCLEO GNSS1A1 and it get position from the GNSS receiver perfectly. When I run the same code on my board, I receive NMEA messages with 0. No position, no speed, no time, 99 satellites..
I attached my schematic. I use chip antenna 1575AT43A0040E. Can anyone help, what is wrong?
2021-07-23 11:41 AM
2021-07-23 11:49 AM
Not going to fish part# out of bitmaps.
Check that your RF amplifier is powered and enabled, check logic state on pins.
You could try injecting RF at various points from a known working GNSS antenna source you've got powered via a splitter.
You could check circuit/antenna tuning with a network analyzer.
Be outside to get the best signals, avoid the human body in proximity to the chip antenna.
Perhaps consult with an ST GNSS FAE
2021-07-23 11:50 AM
Thank you for the answer. Outside the building situation is the same. What do you mean under "Check out antenna connection for the GPS first"?
2023-03-24 3:17 AM
Did you manage to solve it? I'm about to use this GNSS but I'm not sure if it will work with passive antenna
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.