2021-02-03 9:41 PM
Hello ,
in the document : https://www.stmicroelectronics.com.cn/resource/en/application_note/dm00528962-teseoliv3f--i2c-positioning-sensor--stmicroelectronics.pdf
STM32_Nucleo64_F401RE_FirmwareUpdateI2C.bin > for getting NMEA data from GNSS to Host controller over i2c
STM32_Nucleo64_F401RE_FirmwareUpdateUart.bin > for getting NMEA data from GNSS to Host controller over Uart
STM32_Nucleo64_F401RE_I2CBridge.bin > ?
STM32_Nucleo64_F401RE_UARTBridge.bin > for getting NMEA data from hostcontroller to PC over serial UART
Not getting the use of the bold bin(STM32_Nucleo64_F401RE_I2CBridge.bin). Is the understanding for the rest correct?
STM32_Nucleo64_F401RE_FirmwareUpdateI2C.bin > for getting NMEA data from GNSS to Host controller over i2c
>> is the below set of commands does the same - enable the GNSS for fetching data from GNSS to Host controller over i2C?
$PSTMCFGMSGL,3,1,0,0 $PSTMSETPAR,1227,1,2 $PSTMSAVEPAR
in that case what should be the default fw flashed on the GNSS(is UART or I2C)
please clarify
best
2021-02-04 1:32 AM
Hi
STM32_Nucleo64_F401RE_FirmwareUpdateI2C.bin
is the stm32 driver to have firmware update working on stm32 and LIV (when connected over I2C)
STM32_Nucleo64_F401RE_FirmwareUpdateUart.bin
is the stm32 driver to have firmware update working on stm32 and LIV (when connected over UART)
STM32_Nucleo64_F401RE_I2CBridge.bin > ?
is the stm32 driver to have NMEA working on stm32 and LIV (when connected over I2C)
STM32_Nucleo64_F401RE_UARTBridge.bin
is the stm32 driver to have NMEA working on stm32 and LIV (when connected over UART)
2021-02-07 7:00 PM
@Francesco Virlinzi Thanks for answer ,
for case :
STM32_Nucleo64_F401RE_I2CBridge.bin > ?
is the stm32 driver to have NMEA working on stm32 and LIV (when connected over I2C)
do I need to send the below command as well to enable it for i2c??
$PSTMCFGMSGL,3,1,0,0 $PSTMSETPAR,1227,1,2 $PSTMSAVEPAR
if No , what is the prec ondition for the gnss to support this command(in terms of fw flashed)
Br,
Pv
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.