2015-08-20 9:04 AM
Hello,
I am using eMIOS module for SPC560D40L3 MCU for generating PWM. I am using default configuration for the SPCStudio project with no change to FMPLL0 and Clocks settings. My target uses 8MHz external XTAL. With this, I am trying to generate a PWM for frequency ranging from 15Hz to 600Hz. I observed that the PWM channel is not giving exact frequency PWM on the output. The difference is small at lower values but goes on increasing as the frequency rises (@ 125Hz at 600Hz). Why is this behavior for eMIOS module? Is any additional configuration required?Thanks in advance.Mike.2015-08-24 2:29 AM
2015-08-25 7:03 AM
Hello Erwan,
Any updates on this? Your earliest help will be highly appreciated.Thanks.Mike.2015-08-25 8:58 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.