cancel
Showing results for 
Search instead for 
Did you mean: 

Automotive Motor Control using SPC560

Agga
Associate II

Dear all,

Currently, I'm trying to test the SPC560P50L3 MCU for a Motor Control application. I know that I can do it easily by clicking on "import samples from application library". However, every time I try to create the project manually by adding the components like the screenshot below, I always face a lot of errors.

Agga_1-1750735451062.png

 

I noticed that even though I set up the pins in "SPC56xx Motor Control Component," nothing is updated in the pin MAP view, which is not like in the MCSDK versions. In MCSDK, we set up a lot of things in the GUI, like PWM pins, ADC pins, and so on. After that, we can see it also in the CUBE MX after the code generation. However, SPC5 studio is not like that. I'm not sure whether I'm doing something wrong or not. Please correct me if I'm wrong.

I would like to know if there is any step-by-step document or manual to create a custom motor control project in SPC5 Studio.

 

Thanks and regards,

Agga

1 ACCEPTED SOLUTION

Accepted Solutions
Max VIZZINI
ST Employee

Hi,

You should you AutoDevKit Studio and not SPC5Studio. 

Please download it from www.st.com/autodevkitsw 

For a step-by-step approach please refer to the User Manual of our AEK-MOT-3P99081 (or AEK-MOT-3P9908M:(

https://www.st.com/resource/en/user_manual/um2932-getting-started-with-the-aekmot3p99081-cancontrolled-brushless-motor-evaluation-board-based-on-spc560p-and-l9908-stmicroelectronics.pdf

Best Regards,

AutoDevKit Team

View solution in original post

1 REPLY 1
Max VIZZINI
ST Employee

Hi,

You should you AutoDevKit Studio and not SPC5Studio. 

Please download it from www.st.com/autodevkitsw 

For a step-by-step approach please refer to the User Manual of our AEK-MOT-3P99081 (or AEK-MOT-3P9908M:(

https://www.st.com/resource/en/user_manual/um2932-getting-started-with-the-aekmot3p99081-cancontrolled-brushless-motor-evaluation-board-based-on-spc560p-and-l9908-stmicroelectronics.pdf

Best Regards,

AutoDevKit Team

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.