Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SPC58nh-disp - I get a build error when I run the example

Hi, My discovery board is SPC58NH-DISP and I'm a beginner​I want to run the RTOS exampe.​so I tried running the example sequnce.like picture....umm.. I am getting a build error.-----./components/spc5_freertos_tcpip_component_rla/lib/src/FreeRTOS_IP.c...

SHan.4 by Associate
  • 3401 Views
  • 2 replies
  • 0 kudos

Resolved! Floating-Numbers Problem with SPC560P

Hello, I am working with a SPC560P and have a problem with float numbers. As soon as I write a calculation with float numbers in my loop, the loop becomes extremely slow (microsecond range for a simple calculation in the loop).What can be the reason ...

TBles.1 by Associate II
  • 2733 Views
  • 3 replies
  • 0 kudos

Resolved! RX_Callback at SPC560P - Disp

I want to know when or how exactly the RX callback function is triggered on the SPC560P - Disp Discovery board. I have created the function at the low level driver at the serial configuration and see it also in serial_lld_cfg. I have defined it after...

TBles.1 by Associate II
  • 2385 Views
  • 3 replies
  • 0 kudos

SPC5-UDESDK JTAG debugger stopped working after PC was rebooted.

I am setting up a development environment with SPC5-Studio, Discovery Plus Kit for SPC56 L line (with SPC56EL70L5 MCU) and SPC5-UDESDK JTAG debugger.Initially I was able to set up the SPC5-Studio and upload an example application (LED blinker), but a...

KShar.5 by Associate II
  • 3824 Views
  • 7 replies
  • 1 kudos

Spi receive data fault

Hello ​I'm using spc560p40 and I tried to read data from other slave. When I monitor the code on logic analyzer, data is OK, but my mcu saw data one shift to right. I used spi_dll_exchange(&SPID, 2 , TX BUFFER, RX BUFFER) to send and receive data. Wo...

DNewm.1 by Associate III
  • 1126 Views
  • 0 replies
  • 0 kudos