2026-01-12 3:37 PM
Hi,
I'm trying to figure out what to expect for current consumption for the SR5E1E570C30F01X. The datasheet DS13808 - Rev 8 - November 2025 notes under "3.7 Device consumption" that "The following table [table 10] reports each single contributor factor to the device consumption. Refer to Figure 3. Device consumption measurement to see where each contributor is measured.". However, upon inspecting figure 3, it does not contain the required information. Notably, I_DD_HV and I_DD_HV_SMPS_LKG are not shown in the figure despite their grave importance. In fact, only two of the currents listed in table 10 are depicted in figure 3.
Is there a corrected figure or information on calculating the approximate total current draw of the MCU - does the I_TOT calculation under 3.7 truly represent the total current draw, including both the HV and LV side? This is presented in a very unclear way.
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.