Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Problem to execute a TEST application on the SPC56EL70L5

Posted on February 19, 2014 at 03:23Hi, I'm starting to use a SPC56L-Discovery board that I connect with the PC through the SPC5-UDESTK jtag-usb adapter. I installed the SPC5Studio and the UDE 4.0 to debug my board and load programs on it. But I hav...

vittorio by Associate
  • 1545 Views
  • 1 replies
  • 0 kudos

Resolved! ST sibling of mpc563mzp66?

Posted on January 17, 2014 at 22:35With the ST & Freescale alliance and some chips being the same, I wonder if mpc563mzp66 is one of them? If it is, how would I figure out the ST part name? As far as I know it is not as as easy as just swapping the...

arro239 by Senior
  • 1095 Views
  • 1 replies
  • 0 kudos

Include DWARF debug information

Posted on February 05, 2014 at 09:13Dear Sir/Madam,When working with UDE Visual Platform it is possible to view the status of a certain variable. However, in my case it is not possible to view the status of those variables. According to PLS this is ...

SPC5Studio v 2.0

Posted on January 24, 2014 at 17:27Hi, I have downloaded last version of SPCStudio: v. 2.0, this is version written in the web page, but the files refer to version 1.3.1. In past  i have downloaded version 1.3.1, but Help-->About SPC5Studio refer ''...

berardo by Associate II
  • 2475 Views
  • 4 replies
  • 0 kudos

SPC5-UDEDEBG Key not working with SPC5STUDIO

Posted on January 27, 2014 at 15:10Hello,I have ordered and received the following product:SPC5-UDESTK-FULL.This came with a card with a key on it. When I input this key into the website: http://register.hightec-rt.com/ I get the message:Please ente...

Free/Inexpensive TPU Compiler?

Posted on January 08, 2014 at 19:55I would like to start playing with the SPC56 in my free time and would like to use the TPU however I can't afford any of the expensive compilers just for a hobby.Does GCC or another compiler support the TPU? Or do ...

st239955 by Associate II
  • 886 Views
  • 0 replies
  • 0 kudos

C:\SPC5Studio\ude Missing folder

Posted on October 10, 2013 at 15:11I'm evaluating SPC5 studio. I have installed : 1) SPC5 Studio 1.3 downloaded form st site 2) SPC5-UDESTK (128K limited edition) file ude-4-00-09-spc5-udestk.exe downloaded form http://www.pls-mc.com/spc5-udestk In ...

pietro23 by Associate
  • 1358 Views
  • 2 replies
  • 0 kudos

SPC56xxMB EVAL board pinout questions

Posted on November 11, 2013 at 04:06Pad configuration information is needed for the SPC56xxMB EVAL board with the SPC 564AADPT324S mini-module. On the SPC564A (324 pin package), almost all of the eTPU2 and eMIOS pins are multiplexed. For example, on...

Set up ADC triggered by CTU with Tresos on SPC56EL46

Posted on July 10, 2013 at 10:56Hello, I am trying to configure the ADC to be triggered by the CTU. But using a debugger I can see, that many of my configurations made in Tresos are not taken over to the �C registers. As far as I can see the ''init'...

pentti2 by Associate
  • 1600 Views
  • 1 replies
  • 0 kudos

Resolved! undefined reference to `osalThreadSleepS'

Posted on October 31, 2013 at 12:20Hello, i have a question. Bulding CAN code based on example for SPC56ELx produce this error:build/obj/can.o: In function `canStart': can.c:(.text_vle.canStart+0x2c): undefined reference to `osalThreadSleepS' collec...

berardo by Associate II
  • 1568 Views
  • 1 replies
  • 0 kudos