2014-02-05 12:13 AM
Dear Sir/Madam,
When working with UDE Visual Platform it is possible to view the status of a certain variable. However, in my case it is not possible to view the status of those variables. According to PLS this is due to the fact that no DWARF information is included in the .elf file.However, SPC5 Studio has defined -ggdb in the common options and this should include DWARF version 2. However, it seems that nothing is included. I am using the compiler ppc-vle-I am looking forward to your repsonse.Gijs----- edit 20140206-------I have solved the issueWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.