Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! USB Hardware Interface for SPC56XXMB+SPC56ELADPT144S

Posted on July 11, 2013 at 17:35Hello, I have a question. There is a programming USB hardware interface (JTAG)  for evaluation tool (SPC56XXMB+ SPC56ELADPT144S) suggested from ST? #spc56xxmb #spc56eladpt144s

berardo by Associate II
  • 1512 Views
  • 1 replies
  • 0 kudos

Resolved! SPC56EL70L5 and SPC56ELADPT144S mini module

Posted on July 09, 2013 at 14:15 Hello, i have a doubt. The Daughter/adapter board SPC56ELADPT144S is for SPC56xxEL family. In SPC56ELADPT144S datasheet is written:  device supported SPC56EL60L5. But when i search in WEB page for SPC56xxEL famil...

berardo by Associate II
  • 2119 Views
  • 2 replies
  • 0 kudos

Cannot boot from CAN

Posted on June 28, 2013 at 15:41 @page {margin:2cm;} .ExternalClass3D0BC45AD580497FAF99E8CACB84F6C5 P {margin-bottom:0.21cm;} Hi,I have the following setup. I'm using the SPC5604 at 8MHz, FAB and ABS pins are set to boot from CAN. A dedicated...

SPC564Axx OS-Less Test Application problem

Posted on June 07, 2013 at 23:37Hi All,I am unable to get the sample application to run on the dev board.Setup: 1. SPC56xxMB/XPC56xxMB (they are identical according to the schematics)2. SPC564AADPT324S/XPC564AADPT324S (they also are identical accord...

Resolved! How to reset SPC56xxx ?

Posted on May 24, 2013 at 13:48Is any solution to reset CPU writing sequence to register? #spc56-reset #spc560b40x

garik by Associate
  • 3239 Views
  • 3 replies
  • 0 kudos

SPC564A example project

Posted on May 16, 2013 at 16:031. Is there an example project available for the SPC564A? 2. More specifically, is there a SPC5 Studio BSP for the eval board that ST and Freescale jointly sell?3. Is there any support for the eTPU2 in SPC5 Studio and/...

Compile license problem, can you help me?

Posted on March 20, 2013 at 16:05Dear All, I already installed SPC5 studio but I'm having a problem with compile. SPC5 studio is requiring a license. In the installation process I chose the option 30days embedded license but it seemed that it was no...

F0 & IAR5.5

Posted on March 27, 2013 at 17:36Hello,could you please , tell me how to work with F0 in IAR5.5,Thx #iar5.5-fo

SPC563M64 and ST LINK V2

Posted on April 24, 2013 at 10:12Hi,how can i use JTAG in ST-LINK v2 with spc5 studio for flash program mcu spc563M64 ?thank you. #jtag-debugger

Importing existing project in SPC5 studio

Posted on March 16, 2013 at 00:29I'm trying to import into SPC5 Studio a project before built into Standard Eclipse enviroment but is not clear what should i do. Should i import it as standard eclipse project or as SPC5 studio project? Thanks