Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

C90FL (beta) flash program fails - help!

Posted on June 20, 2014 at 11:41C90FL program fails due to alignment error but all parameters check out?Parameter details before call:dest       size       source     result = C90FL_ERROR_ALIGNMENT0x00008000 0x00000100 0x40005300 0x000001000x0000810...

Resolved! SPC5Studio (V3-V2) Can not Code Generated for SPC560Bxxx

Posted on June 11, 2014 at 14:55 Hello, I'm trying to create new project (Starting Code Generating) with SPC5 Studio Version (2 or 3) for SPC56B/Cxx Series. But It doesn't generated. SPC5 Console Out: Begin processing component re...

Getting C90LC library for spc560b64l

Posted on June 16, 2014 at 12:07spc560b64l ssd flash api with eval of spc5?Hi,Re=post since no reply - Cheers ST!I am using an evaluation of SPC5 and want to start playing with the flash controller in mcu, my device is spc560b64xxx.I have read about...

SPC5 Studio V3

Posted on June 01, 2014 at 08:06Is SPC5 Studio V3 available? Based on http://www.st.com/web/en/catalog/tools/PF255702 it would indicate V3.0 is available, but download from SP store is V2.0, files dated 12/10.2013. What new features are planed for V...

Problem importing example project

Posted on May 27, 2014 at 10:43Hi, I downloaded example software SPC56EL and successfully imported all of them but then i can't get them compiled. I don't know how to set current toolchain and current builder, keeps giving me make error about object...

Resolved! SPC564B70 (Bolero) Power Draw in Standby Mode

Posted on May 23, 2014 at 19:21Can anybody offer any knowledge of using STANDBY mode?  I am putting the chip in STANDBY and it appears to go there, as the processor goes dormant until I cause a wakeup event.  But the current draw on the VDD_LV powe...

Resolved! XPC560BADPT208S Documentations

Posted on May 06, 2014 at 16:49Hello,I am searching for XPC560BADPT208S mini module realated docs, but i can't found it, any help of any related docs is higly appreciated. 

SPC560D40L1 - ADC does not finish sampling

Posted on April 03, 2014 at 12:21Hi, I'm trying to setup an analog conversion on SPC560D40L1. I activated the ADC in HAL configuration, defined a adc-conversion-group that consists of channel 0 (ADC1_P[0] on Pin PB4). The ADC does not finish the sa...

sp by Associate II
  • 3258 Views
  • 7 replies
  • 0 kudos

PWM with eMIOS on group0 ch 0..5

Posted on March 31, 2014 at 20:03Hi, it's my first Project with a SPC560D40 an SPC5 Studio. I'm trying to generate PWM-Signals on the Pins RA0 to RA5. When I look in the eMIOs Settings of the SPC560Dxx HAL Driver Component, I can only activate eMIOs...

sp by Associate II
  • 1491 Views
  • 2 replies
  • 0 kudos

ARM Cortex A8,A9 processor 1GHz

Posted on March 19, 2014 at 12:34I do not know why ST does not have GHz range Cortex A8 processors like TI,freescale,samsung,...? I think ST can produce them with low cost of samsung but at the quality of freescale or better. ST have stm32 in cortex...