Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SPC560P40 eDMA feeds CRC engine. Wrong CRC values produced

Posted on April 08, 2015 at 17:10I am hoping someone has experience using the CRC engines with success.  I am feeding the CRC input register with 32 or 16 or 8 bit sizes of the same data and the CRC produces different outputs.  I have to be doing so...

erreur mac adresse (spc5studio)

Posted on May 25, 2015 at 11:51Hello,I connected to licensing website (http://register.hightec-rt.com/) , to get the license file of spc5studio .But I make an error in my MAC address: I write BB-CA-3A-73.57.85 but the correct MAC address is B8-CA-3A...

Wakeup signal

Posted on May 18, 2015 at 11:05Hello,I am trying to configure a wakeup signal WKPU6 as below.WKUP.WISR.B.EIF = 0x02000000; //Clear interrupt flagWKUP.WIREER.B.IREE = 0x02000000; //Disable rising edgeWKUP.WIFEER.B.IFEE = 0x02000000; //Enable falling ...

ssk by Associate II
  • 1597 Views
  • 2 replies
  • 0 kudos

Resolved! Monaco Pin Assignment_PA

Posted on May 08, 2015 at 04:52Hi. while I am reading SIU PCRxx for Pin Assignment in RM0015 SPC563Mxx Reference Manual, It is not clearly described about Pin Assignment PA[2:0] value. eg. SIU_PCR179. what is value of PA[2:0] for each function of eM...

270284440 by Associate III
  • 1082 Views
  • 1 replies
  • 0 kudos

FlexCAN filter duplicated on all configurations

Posted on May 12, 2015 at 14:11Hello, I'm using both FlexCAN of SPC56EL60 on SPC5 Studio 3.4.3 and I wanted to define filters for each of them. I created a config for each of them containing different filters. CAN1 has 16 filters from 0x200 to 0x20F...

PWM configuration structure

Posted on April 03, 2015 at 08:01I am using SPC560D40L3 with SPC5Studio. I am trying to generate a PWM signal. Using Application configuration, I configured the HAL drivers to generate a PWM of 5Hz. Here, I configured the clock frequency and period ...

ssk by Associate II
  • 2817 Views
  • 7 replies
  • 0 kudos

Application Import - file system

Posted on May 12, 2015 at 08:38I am trying to import settings/files from another project to current project. I followed the steps as File->Import->General->File System and provide the path for source project and click finish. Tool is giving an error...

ssk by Associate II
  • 1991 Views
  • 3 replies
  • 0 kudos

[solved] SPI slave configuration for SPC56EL

Posted on March 26, 2015 at 10:17Hello, I would like to implement a SPI communication between an SPC560D and an SPC56EL Discovery Board. The SPC56EL should act as slave, the SPC560D as master. For both boards, I am using the corresponding DSPI examp...

Patriks by Senior
  • 3479 Views
  • 9 replies
  • 0 kudos

make: *** No rule to make target `all'. Stop.

Posted on April 30, 2015 at 15:17got errors compiling all projects created by wizard:**** Build of configuration Default for project SPC56ELxx OS-Less Test Application for DiscoveryPlus ****make -j2 all make: *** No rule to make target `all'.  Stop....

oleg2399 by Associate
  • 2319 Views
  • 3 replies
  • 0 kudos