2015-05-19 4:28 AM
I wonder if it is possible to generate C Code with the PinMap Wizard for use with the Multi IDE Green Hill Compiler and if that is possible how to integrate the code to a Multi IDE Project?
Thanks in advance, Dominik2015-05-21 2:48 AM
palInit(&pal_default_config);
and
/* Initial setup of all defined pads, the list is terminated by a {-1, 0, 0}.*/
static
const
spc_siu_init_t spc_siu_init[] = {
{PCR(PORT_A, PA_BUTTON), PAL_LOW, PAL_MODE_INPUT_PULLUP},
{PCR(PORT_B, PB_LIN0_TDX), PAL_HIGH, PAL_MODE_OUTPUT_ALTERNATE(1)},
{PCR(PORT_B, PB_LIN0_RDX), PAL_HIGH, PAL_MODE_INPUT},
{PCR(PORT_A, PIN_GPIO2), PAL_LOW, PAL_MODE_INPUT},
{PCR(PORT_B, PB_TRIMMER), PAL_LOW, PAL_MODE_INPUT_ANALOG},
{PCR(PORT_A, PIN_GPIO3), PAL_HIGH, PAL_MODE_INPUT},
{PCR(PORT_C, PC_LED8), PAL_LOW, PAL_MODE_OUTPUT_PUSHPULL},
{PCR(PORT_C, PC_LED7), PAL_LOW, PAL_MODE_OUTPUT_PUSHPULL},
{-1, 0, 0}
};
/* Initialization array for the PSMI registers.*/
static
const
uint8_t spc_padsels_init[SPC5_SIUL_NUM_PADSELS] = {
0, 0, 0, 0, 0, 0, 0, 0,
0, 0, 0, 0, 0, 0, 0, 0,
0, 0, 0, 0, 0, 0, 0, 0,
0, 0, 0, 0, 0, 0, 0, 0,
0, 0, 0, 0, 0, 0, 0, 0,
0, 0, 0, 0, 0, 0, 0, 0,
0, 0, 0, 0, 0, 0, 0, 0,
0, 0, 0, 0, 0, 0, 0,
};
/**
* @brief PAL setup.
*/
const
PALConfig pal_default_config = {
PAL_MODE_UNCONNECTED,
spc_siu_init,
spc_padsels_init
};
Best Regards
Erwan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.