Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Bug on Pinmap in SPC560B50L5 for set PWM

Posted on April 23, 2015 at 10:11Hi I want to Emios-0 in SPC560B50L5 these Specific Pin (PB[11],PB[12],PB[13]) but when i set these pin in pin map as output like E0UC4 or E0UC5 ,... the pin map set the ANX Pins . and i check in spcstudio for use th...

SPC560D30L3 - Serial driver

Posted on March 17, 2015 at 16:11Hello,I am trying to use the serial driver for SPC560D30L3 device using Discovery kit (I have replaced SPC560D40 with SPC560D30 MCU). When I try to configure the 'Serial Driver Settings' for buffer size, it only acce...

ssk by Associate II
  • 2251 Views
  • 9 replies
  • 0 kudos

Resolved! SPC5 test application - No rule to make target 'all'

Posted on March 31, 2015 at 14:41Hi there,I have SPC5 studio installed and I updated all the components available (so my core and app wizard are 3.4.3). I am trying to run OS-less CAN test application from the wizard, having chosen the EVB I have (t...

gilad2 by Associate II
  • 3385 Views
  • 6 replies
  • 0 kudos

Full documentation for SPC560P - DISP?

Posted on March 12, 2015 at 15:35Hello,I need a full documentation for the header I / O of this board (SPC560P - DISP). Is there? The manual on the site of St. explains only the configuration, but not their role. I need connect an LED to a breadboar...

gl2 by Associate III
  • 5989 Views
  • 10 replies
  • 0 kudos

SPC560B-DIS Watchdog Issues

Posted on April 13, 2015 at 11:42Hello,I am currently trying to set up the Watchdog on my SPC560B board.Firstly, after enabling the watchdog and letting it time-out into a reset, it then enters SAFE mode and does not reset the program. RGM.DERD is s...

jleech92 by Associate
  • 1530 Views
  • 2 replies
  • 0 kudos

SPC560D30L3 - ADC states

Posted on March 18, 2015 at 15:55Hello,I am trying to use the ADC driver (ADCD2) for SPC560D30L3 device using Discovery kit (I have replaced SPC560D40 with SPC560D30 MCU). I am trying to implement a state machine using different states of ADC driver...

ssk by Associate II
  • 4682 Views
  • 11 replies
  • 0 kudos

Application Configuration - Clock settings

Posted on April 25, 2015 at 13:58I am using test application for serial interface with SPC560D30. I used the application configuration - clock settings as 16MHz with the SPC discovery kit. Now keeping the test application same, I want to change the ...

ssk by Associate II
  • 3569 Views
  • 3 replies
  • 0 kudos

Facing issue with LINFLEX_0: Help needed

Posted on April 23, 2015 at 17:36Hi,I am writing a LINFLEX_0 driver for SPC560B60L3. DMA is not used as of now. All interrupts are disabled.Linflex_0 can be configured in 2 sets of port pins set 1: LIN0TX in PB[0] and LIN0RX in PB[1]. Alternate func...

saswatkd by Associate II
  • 2173 Views
  • 3 replies
  • 0 kudos

Resolved! [solved] Interrupt priorities

Posted on November 25, 2014 at 13:18Hello, Yesterday, I investigated a problem with my software project for an SPC560B. There are several calculations running on the controller and it additionally communicates over UART with a PC. When I tried to in...

Patriks by Senior
  • 4363 Views
  • 16 replies
  • 0 kudos

SPC5Studio Login information

Posted on April 15, 2015 at 08:00I am using SPC5Studio with SPC560D MCU for a long time. From couple of days back, when I start the SPC5Studio application it asks for the login information (user name and password) for three different urls. Please fi...

ssk by Associate II
  • 2310 Views
  • 5 replies
  • 0 kudos