Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SPC560B60, SPC560B64 and ''Freescale SPC5607B'' compatibility

Posted on December 07, 2015 at 12:46Good morning, I've 2 questions: First, I'm wandering about the differences between: the SPS560B60 and the SPS560B64? Are they compatible in the sense that the same code would run the same in both devices? (I'm alr...

mbahtat by Associate
  • 1049 Views
  • 1 replies
  • 0 kudos

using UART

Posted on November 27, 2015 at 11:13Hello everybody, I'm using the SPC56EL70L5DISP board.In order to use UART, I put the jumpers in J18 and J20 to connect UART-MCU LIN0, following the board user guide.Running the test example with UART and blinking ...

eDMA with SPC560B

Posted on November 30, 2015 at 16:05Hi all, I try to get the eDMA Modul working. My starting point is an example code from the document ''Qorivva Simple Cookbook “Hello World�? Programs to Exercise Common Features on MPC5500 & MPC5600 Microcontrolle...

dominik2 by Associate II
  • 1937 Views
  • 2 replies
  • 0 kudos

Using SRAM

Posted on October 30, 2015 at 12:43I am using SPC560D with SPC5Studio. I want to save the device configuration/status before putting the device to standby mode and use/retrieve this status when the device exits standby mode. Can this be achieved by ...

ssk by Associate II
  • 2537 Views
  • 6 replies
  • 0 kudos

SPC5Studio 3.7.1 is available !!!

Posted on November 24, 2015 at 10:24Dear All , SPC5Studio 3.7.1 is available *** Highlights *** - Documentation Update (Pinmap, ClockTree, SPC5Studio userguides) - Several bugs and improvements, please refer to https://my.st.com/public/STe2ecommuni...

eMIOS overflow callback and frequency range

Posted on October 19, 2015 at 12:20Hello, when I was working on SPC56EL with older SPC5 Studio versions, the overflow callback was called only when the internal counter was overflowing. This was perfect to detect too low frequency which can't be mea...

Updates

Posted on November 10, 2015 at 15:44Hello everybody,I tried to update SPC5 studio but i got the error ''No repository found containing:''on every update package.Trying to fix this problem I accidentally erased repositories.Now i need to know what si...

SPC5UDESTK - Checksum

Posted on October 07, 2015 at 14:48I am using Universal Debug Engine v4.02.07 for programming the flash with SPC560D MCU with PLS USB/JTAG adapter. Where can I find the checksum value for the obj file (.elf or .hex or .out)? Which menu of the tool h...

ssk by Associate II
  • 2234 Views
  • 4 replies
  • 0 kudos

SPC5Studio 3.7.0 is available !!!

Posted on September 18, 2015 at 13:51Dear All ,SPC5Studio 3.7.0 is available*** Highlights ***- SPC563Mxx RLA (Register Level Access) drivers for Monaco, with sample applications and related documentation - EEPROM emulation software, with sample app...