cancel
Showing results for 
Search instead for 
Did you mean: 

SPC560B60, SPC560B64 and ''Freescale SPC5607B'' compatibility

mbahtat
Associate
Posted on December 07, 2015 at 12:46

Good morning,

I've 2 questions:

First, I'm wandering about the differences between: the SPS560B60 and the SPS560B64? Are they compatible in the sense that the same code would run the same in both devices? (I'm already aware of FLASH/RAM memory sizes difference, is there any other difference?).

Second, how much compatible a code that was running into the ''Freescale SPS5607B'', would run into the ''ST SPS560B60'' ?

Many Thanks.

Kind Regards.

#spc560-mcu
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Erwan YVIN
ST Employee
Posted on December 07, 2015 at 14:34

Hello ,

the difference is just the flash size.

1M (for 60) 1.5MB for 64

you can use the same code.

you have to just to check your mapping LQFP100 / LQFP144

the code ''Freescale SPS5607B'' (1.5 MB) is compliant for B60 and B64.

it is the same device.

    Best regards

                Erwan

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.