cancel
Showing results for 
Search instead for 
Did you mean: 

SPC5Studio 3.7.0 is available !!!

Erwan YVIN
ST Employee
Posted on September 18, 2015 at 13:51

Dear All ,

SPC5Studio 3.7.0 is available

*** Highlights ***

- SPC563Mxx RLA (Register Level Access) drivers for Monaco, with sample applications and related documentation 

- EEPROM emulation software, with sample applications and related documentation 

- Saving and restore Pin map wizard settings 

- Added FlexCAN2 support for SPC56EL70L5 MCU (Leopard)

- Marketplace features enabled with official http web address

Bugs fixing:

-  fixed a problem on the Pinmap Wizard for SPC56ECxx MCU (Bolero 3M) 

-  fixed issue on FlexCAN1 on SPC563Mxx MCU (Monaco)

-  watchdog threshold issue solved for ADC driver for SPC56P/L/B/D/C MCU 

-  fixed issue for SCI driver for SPC56M/A MCU 

-  Minor cosmetic changes for nil OS, CRC, eTimer2  test applications for SPC56L/B/D/C MCU

- Several bugs and improvements, please refer to 

https://my.st.com/public/STe2ecommunities/mcu/Lists/SPC5%20Studio/AllItems.aspx

(when the forum will be available)

*** Notes ***

- Make sure to read the SPC5Studio Users Guide and Components

Writers Guide in

the help section.

Enjoy SPC5Studio,

The SPC5Studio Team.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
lizheng887
Associate II
Posted on October 28, 2015 at 07:03

Hi,

where to download the latest version v3.7.0?

The ST.com still display v3.5.

Nickname2551_O
Associate III
Posted on October 28, 2015 at 09:02

Hi Michael,

please note that SPC5Studio is delivered in two different ways, depending on the changes. Major changes are delivered in a full installer that you can download from ST.com, while less important changes are delivered through Eclipse update site mechanism.

New users have to download first the latest major version (in your case version 3.5), then update it (each time SPC5Studio is launched a check for updates is done, that you can accept or refuse).

Hope this helps

Best regards

Philippe

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.