Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! Initialization MCU

Posted on January 22, 2017 at 12:34 Good day. This my first application on spc5 studio. I add for testing one led on Port B[1] to board witch MCU SPC560P40L3. I add in generate main.c file one sting -pal_setpad(PORT_B, LED_RED);. Pin will add p...

0690X0000060Mq1QAE.jpg 0690X00000603SwQAI.jpg 0690X00000603SxQAI.jpg

Impossible to download SPC5Studio

Posted on March 23, 2016 at 09:29Dear All ,there is a bug in our lovely corporate website.it is not possible to download SPC5Studio by http://www.st.comour IT is trying to solve the issue as soon as possible.             Best regards                ...

Distinguish occurrence of framing error in LINflex Module

Posted on January 12, 2017 at 09:44Hello,we are currently working on a LIN-Slave Driver for the SPC560D40L1. The use of the hardware-id-filter have made it easy so far but now we fail in one last test where we must distinguish whether the framing er...

torben by Associate II
  • 4914 Views
  • 11 replies
  • 0 kudos

Information on patch.xml workflow

Posted on November 18, 2016 at 17:38 I'm currently using SPC5Studio 4.2.1 (4.2.1.201607051420) and use it to develop on an SPC560B-DIS evaluation board. I noticed that edits I make to component files in the lib sub-directory are handily stored i...

eSCI and Virtual COM Port (PLS) for SPC653M

Posted on January 10, 2017 at 20:40Hi,I have some problems with serial communication with my board. Could someone help me, please?I have an SPC563M board with SPC5-UDESTK (pls) for debugging. Is this device designed for Serial trasmission by virtual...

SPC5-Flasher download link error

Posted on January 09, 2017 at 15:10my.st.com DOWNLOAD LINK ERROR: SPC5-Flasher download link is pointing to the old v1.0.3 of uFlasher instead of the v2.6.1 from SPC5-Flasher...

CAN / CAN-Open / UART Bootloader?

Posted on June 26, 2015 at 16:50Hello, I can't find any application note regarding bootloader on SPC56. I'm looking for CAN or CAN-Open or even uart bootlader to reflash my SPC56EL60. Any advise is welcome! Thank you.

Protect MCU From Read & Write

Posted on December 24, 2016 at 18:37HiI use SPc560B54L5How can i protect the controller from reading the program?and how can i set the locks directly in Program?ThanksBest RegardsNazerian Vaniam

Resolved! expired license error

Posted on January 02, 2017 at 16:09Hi I used to work with SPC5Studio with a permanent license. Now I have a license error:make all Compiling boot.s./components/spc560bxx_platform_component/lib/src/boot.s:1:0: internal compiler error: initialising li...

rim sari by Associate
  • 1967 Views
  • 3 replies
  • 0 kudos

Beginner guide for SPC563M

Posted on December 25, 2016 at 19:54Hi,I have got a spc563m board and I have installed spc5studio to program it, but i don't know which library i should use  and how to use the chosen one. I don't know the pinout and basic methods, yet. Is there a g...