Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Pin Description on SPC582B60E1

I need to find a pin desription on SPC582B60E1. I haven't found it in datasheet on SPC582Bx series, but i found the SPC582B - discovery board schematic with some details.Can anybody provide necessary info?Thanks!

IBaba by Associate
  • 857 Views
  • 0 replies
  • 0 kudos

How to connect SPC58NG-DISP to my laptop?

Hi all,Recently we have purchased the SPC58NG-DISP evaluation board. I want to connect it to my laptop to deploy new SW on it using the SPC5Studio.My question is, how to do that? Can I just connect it using the serial board? Or I have to buy another ...

MNabi.1 by Associate
  • 1014 Views
  • 1 replies
  • 0 kudos

Problem of converting groups (ADC) with SPC56EL70L5

Hi,I write in this forum for a problem with the ADC of the microcontroller SPC56EL70L5.My goal is to perform two group conversions in ADC0 and wo in ADC1.I use the function generated by the program "adc_std_start_conversion" but some values ​​obtaine...

ADC of SPC560B Discovery Board-(internal voltage)

Hi,I am using SPC560B discovery board .I am using ADC1. The jumpers J4, J7 are shorted to get the internal voltages. But the internal volatge is not constant all the time, there are some variations. Because of that i get variations with the output v...

SEphr by Associate II
  • 676 Views
  • 0 replies
  • 0 kudos

Resolved! SPC5 crypto lib sample code

Hi all, I have downloaded the crypto lib directly from the "Help->Install New Software" menù of SPC5Studio , but I do not have any idea on how to use it, include it inside a project, use sample codes (if available), and so on.Proposed link:https://my...

AMocc by Associate II
  • 3634 Views
  • 3 replies
  • 0 kudos

can't communicate with target processor

HI, I'm having PEMicro USB-ML debugger and try connecting it with SPC560B-DIS board.But I'm not able to connect with the target. I could able to see both target power and USB power glowing in the USB-ML hardware.As well, I updated the PROGPPCNEXUS f...

0690X000009jAmQQAU.png 0690X000009jAmLQAU.png 0690X000009jAmGQAU.jpg

UART baud 115200 issue!!

Hi,  I'm using SPC560B54L5 Discovery board.  I'm trying to get serial communication to work at baud rate 115200. And it works well with other baudrate like 9600,38400 and 57600.#define SPC5_PERIPHERAL1_CLK_DIV_VALUE   2U#define SPC5_LINFLEX0_CLK   (S...

SEsak by Associate
  • 1592 Views
  • 1 replies
  • 0 kudos