Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SR6G7 programming with StellarLink in a batch mode

I'm trying to download SR6G7 elf code into internal Flash. So far this MCU seems to be not directly supported from the StellarStudio (?).Is there a way of programming my board using StellarLink from the command line? I found a working solution for ot...

savo_0-1705997531385.png savo_1-1705998185811.png
savo by Associate
  • 2387 Views
  • 2 replies
  • 0 kudos

Query in FMEDA Analysis performed for SPC58xNx

We are implementing application software in performance core. So, we are bound to do FMEDA analysis,  *   Is there a FMEDA analysis performed in SPC58xNx hardware from your side?  *   All failure detections which are carried over in performance cores...

SP.4 by Associate
  • 701 Views
  • 1 replies
  • 1 kudos

Resolved! Stellar E vs Stellar P for inverter

Hello, I am interested in the Stellar E and P series for the purpose of motor control, with an inverter topology that has 12 independent switches and requires fine control of the offset between some of the waveforms.1) The E series is marketed as opt...

ay by Associate
  • 1384 Views
  • 2 replies
  • 0 kudos

SPC560P-DISP CAN TX

I've got the CAN Test app loaded and working as it should. I'm trying to get it to transmit out instead of loopback. I've already uncheck the option for loopback and simplified the code to only transmit. However, I don't see any activity on the CAN p...

BXS by Associate II
  • 1487 Views
  • 6 replies
  • 0 kudos

Getting started with SPC560P-DISP

Just got an SPC560P-DISP and I'm following AN4487 Getting started instructions. I have the board connected via USB to my computer and I've got SPC5Studio up and running with a Serial Test App. I have cleaned, generated and compiled the app. Following...

BXS by Associate II
  • 795 Views
  • 0 replies
  • 0 kudos