Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC570 CAN outputs bad frame, independent of frame parameters

Hello,I am currently trying to transmit CAN frames from my SPC570S-DISP board. The board is connected to a verified working CAN node that is expecting frames at 500 kbps. I am able to write to the CAN buffers and get the CAN core to transmit, but it ...

0690X000008wDBxQAM.png
AZayt.5 by Associate II
  • 4550 Views
  • 7 replies
  • 2 kudos

Resolved! Hello Dear ST Community I am Salih, Electrical Electronics Engineer and Software Developer. I am developing software for functional security in the automotive industry in a company.

For this reason, we need an Eval Board that meets the requirements I will list below. I request your suggestion equipment.Thank you,Requirements;There must be a debugger for the uC on the development board.uC must have Ethernet, FlexRay, USB, SDHC, C...

MKara.7 by Associate
  • 1418 Views
  • 1 replies
  • 0 kudos

Resolved! I want to connect to the SPC584B-DIS with SPC5Studio, however I always get the following error when trying to validate a project on the board: "LOAD ERROR: STM32 - no connected board(s), invalid firmware or the board should be re-started"

Hello,I am currently trying to run a Machine Learning application on the SPC584B-DIS MCU. I used SPC5Studio with the AI plugin to create the project and it compiled without an error. The board is connected to the PC by USB cable. When I try to valida...

FDado.1 by Associate
  • 1395 Views
  • 1 replies
  • 1 kudos

Resolved! Frozen ADC Bits in Debug Mode

Hello,How can I watch the values of global or static variables for ADC Module. When I add the variables which keeps data to the watch table, I dont see what's going on. They don't change. ( Also I wanna learn this for Timer and other Modules)

Msert.1 by Associate III
  • 2046 Views
  • 3 replies
  • 0 kudos

How to configure HTTP/FTP example

Hello folks,I'm playing around with the SPC58 discovery kit and trying to setup the HTTP/FTP worked example. It doesn't appear to me that out of the box that FTP nor HTTP code on the target runs correctly. I can ping the discovery kit, so clearly the...

RSmit.12 by Associate II
  • 1436 Views
  • 1 replies
  • 0 kudos

Resolved! SPC574S Dead-Time

Hello,1) Where is the reference manual of SPC574S-DISP. I could not find it. What will I take reference for programming?2) I want to create dead time on my PWM signals. I know how to create a PWM signal. How to add dead time to PWM signals.Regards,

Msert.1 by Associate III
  • 2344 Views
  • 3 replies
  • 0 kudos