Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC574S CAN communication failed。

When I test CAN whether it can send data successfully。 I found it always ​failed. Now I use 100pin SPC574s. I have configured can tx PB0(18),PA15(17)pin. I test using SPC5Studio 6.00 version. please help me check my project. Thanks a lot.

wminx.1 by Associate
  • 1235 Views
  • 1 replies
  • 0 kudos

Resolved! Command line operations with the SPC5Studio

Hi,With SPC5Studio 5.8.1, is there a command line option to generate the SPC5 application? Or a headless way to generate and build the project?I'm looking into non-GUI interactions with the environment so that generation and building can be scripted....

GKove by Associate
  • 2516 Views
  • 4 replies
  • 0 kudos

Resolved! How to do SPI + DMA?

Hi:I know how to use SPI;but, i want SPI+DMA, How to configure?Is there a sample code?

SLEE.6 by Associate II
  • 2262 Views
  • 2 replies
  • 0 kudos

Resolved! SPC574S Reference Manuel

Hello, I need this document as soon as possible. I could not find anywhere.Regards

Msert.1 by Associate III
  • 1463 Views
  • 1 replies
  • 0 kudos

Resolved! DMAMUX configuration example for periodic triggering

Hi all,I seem not to be able to achieve periodic DMA transfers using DMAMux periodic triggering functionality.I read on SPC574Kx reference manual that (§7.3.9.2)DMAMUX1 receives PIT_0 Trigger 0-4DMAMUX2 receives PIT_0 Trigger 5and that (Table44):PIT_...

CoolMo by Associate III
  • 2332 Views
  • 2 replies
  • 0 kudos

Resolved! BDSL File Request

I would like to request the BDSL file for PN#SPC58NN84E7RMHBR.Can someone help to check and advise?Thanks.Regards,Kent

KLiew by Associate
  • 1369 Views
  • 2 replies
  • 0 kudos

Resolved! CI Build Options

Hello, Has anyone successfully implemented headless builds for SPC5 studio? I am looking for information on this with the intent on creating a docker image to build new binaries at each commit with the usage of bitbucket pipelines. Any assistance wou...

NMazz.1 by Associate II
  • 2275 Views
  • 4 replies
  • 0 kudos

Resolved! SPC58xNx : ECC Error Injection in DFlash

My requirement is to 1) Inject ECC error in DFlash2) ECC has to be detected, but there should not be any reset as it occurred in DFlashWhat are the registers to be set for the above steps?Note : I tried sample programs from SPC5Studio* FCCU Test Appl...

SP.4 by Associate
  • 1065 Views
  • 1 replies
  • 0 kudos

Resolved! SPC58xNx : ECC Error Injection in DFlash

SPC58xNx : ECC Error Injection in DFlashMy requirement is to1) Inject ECC error in DFlash2) ECC has to be detected, but there should not be any reset as it occurred in DFlashWhat are the registers to be set for the above steps?Note : I tried sample p...

SP.4 by Associate
  • 1314 Views
  • 1 replies
  • 0 kudos