Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SPC58 Network RLA/DHCP Issue

I had a functioning TCP/IP application I am trialing on the SPC58EC-DISP discovery board using DHCP. SPC5Studio pulled updates and is not forcing me to migrate to the latest RLA (1.8.2.20200908161300) which breaks some network code -- this was fixed....

VMiki.1 by Associate II
  • 4150 Views
  • 5 replies
  • 0 kudos

Resolved! Reference Manual SPC574S60E3

The SPC574S60 microprocessor only has e book file. I can't find the reference manual. Please help me.

AATAY.1 by Associate
  • 2030 Views
  • 2 replies
  • 0 kudos

ADC and DMA

Hello,In the SPC5Studio, eDMA comes enable defaultly. My question when I enable ADC Module, conversion of analog channel is done through eDMA ? If not should I need doing some configurations ?Best Regards,

Msert.1 by Associate III
  • 1994 Views
  • 2 replies
  • 0 kudos

SPC5 studio user manual

Hi everyone, we are working on BLDC motor driver development for E-cycle and E-bike for that we choosen a controller SPC560P controller in that are going to use FOc algorithm and our application for that we want to generate some basic peri...

Resolved! SPC560D CAN baudrate confirmation

Hello all,im working on a project that uses an SBC, using my logic analyser i can confirm data is coming and and looks to be a can signal but it seems my baud rate timing is incorrect or something else is amiss.my board is the SPC560DL1, i understand...

0693W000004JohiQAC.png 0693W000004Joi2QAC.png 0693W000004Joh9QAC.png 0693W000004JohEQAS.png
AndreasPA by Associate III
  • 2051 Views
  • 7 replies
  • 0 kudos

The STM2 can not jump into ISR

my dear guys, I want to take use of STM_2 as a system tick for OS schedule, but when the condition for STM_2 compare interrupt satisfied , the PC can not jump into ISR ,the PC jump into a illegal position.thanks pretty much for your suggestions.

0693W000005APfYQAW.png 0693W000005APfnQAG.png
Yqiu.1 by Associate II
  • 1565 Views
  • 2 replies
  • 0 kudos

Resolved! Multi-Core Questions

Hi,It is a SPC56EC Dual core sample project which comes with SPCStudio (I imported the project form your library) and I have some questions. The screenshot is attached.1- When we use dual core at the same time, how do they memory sharing? They share ...

0693W000005B5zpQAC.png
Msert.1 by Associate III
  • 1362 Views
  • 2 replies
  • 1 kudos