Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SPC582B-DIS with the VNF1248 Evaluation board GUI

Dear ST Community,I recently bought the SPC582B-DIS board in order to test the EV-VNF1248F board. I installed the VNF1248 Evaluation board GUI and the UDE STK 2021 by following VNF user guide.I downloaded the Chorus1M_VNF1248_discovery.elf in order t...

Resolved! Sr6p3e issue with Gicr module r/w

I am using sr6p3e and I tried to access Gicr registers but I got aport exception, I tried several things like check if clock control the module and if there is a protection registers but I didn't find anything, I know that it use axim for interface s...

1000064251.jpg 1000064250.jpg
Safifi by Associate
  • 222 Views
  • 1 replies
  • 0 kudos

SPC582B, IVOR0 Issue

I am developing using AutoDevKit and SPC582Bxx.When the device wakes up from STANDBY0 to WKPU, it jumps to IVOR0.This occurs when the Trace32 debugger is connected during wake-up.I would appreciate your advice on if there are any specific settings I ...

John_Lee by Associate
  • 150 Views
  • 0 replies
  • 0 kudos

stellarstudio debugging issue on SR5E1-EVBE7000P board

Hi Team,   I am facing to connect with SR5E1-EVBE7000P board. I give below the issue. Can anyone help me to resolve this issue   Error in final launch sequence:   Failed to execute MI command: -exec-run Error message from debugger back end: Don't k...

sai1996 by Associate II
  • 2188 Views
  • 6 replies
  • 0 kudos

Bootloader example files for the SR5E1E5

Hi Do any example bootloader files exist for the SR5E1E5 micro series.  I can see that there are flash examples in the ESDK area of the StellarStudio, but I cannot find any bootloader example files. If there is no example code, then are there any app...

PaulW by Associate
  • 124 Views
  • 0 replies
  • 0 kudos