AutoDevKit Ecosystem

Ask questions and find answers on the AutoDevKit solution. Discuss voltage configurations, motor control, and AutoDevKitStudio programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Urgent help! Regarding the AEK-MCU-SPC5LNK debugger issue!

Hello! I bought 2 AEK-MCU-SPC5LNK debuggers to download the program for the AEK-MOT-MR200G1 development board! But during use, a prompt as shown in the following picture will appear! I don't know if it's a device issue or something! The AEK-MOT-MR200...

QQ图片20240527120146.jpg QQ图片20240527120150.jpg QQ图片20240527120154.jpg
Bwang.3 by Associate III
  • 1240 Views
  • 1 replies
  • 0 kudos

Resolved! SPC58EC No JTAG client found ! in windows 10

Dear community members, I am following the tutorials from ST via: https://www.youtube.com/watch?v=4Vn_cRUfRag&list=PLnMKNibPkDnEju3j_qhe-MFK-NnwD_kuP&index=7&ab_channel=STMicroelectronics I am currently using SPC58EC but when I load workspace from UD...

trishuynh_0-1716714115632.png trishuynh_1-1716714144960.png
trishuynh by Associate III
  • 4327 Views
  • 3 replies
  • 0 kudos

Resolved! How to add extra memory to the AEK-AUDC1D9031 board

hi 1. on AEK-AUDC1D9031 there is SPC582B60E1 MCU with 1 Mb flash.2. i want to more wav files to play. but SPC582B60E1 is has only 1MB.3. so that i want to know how to integrate the extra memory to the  AEK-AUDC1D9031 board.4. how to connect external ...

Resolved! In "aek-AUD-C1D9031" - AVAS project the NOISE is high when I use PIT Timer Interrupt.

hi community,                      I am using the "Avas Compact - Test Application" example code which is provided in the AUTODEVKIT.  I had extended that example code with PIT (the frequency is 1sec). after adding the PIT the WAV files are playing w...

Resolved! want to know the CAN BUSOFF is implemented or not In "Avas Compact - Test Application".

hi community,                      I am using the "Avas Compact - Test Application" example code which is provided in the AUTODEVKIT. hear I enabled the CAN communication and it is working fine. but i want to know CAN BUSOFF is implemented or not in ...

Resolved! Timeout functions

Hi community,I have implemented AVAS, I am getting the output as expected but with one issue that even after I stop communication in the CANoe , I am getting the sound continuously.I wanted to know two things1. Do we have any API that stops the sound...