AutoDevKit Ecosystem

Ask questions and find answers on the AutoDevKit solution. Discuss voltage configurations, motor control, and AutoDevKitStudio programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Pin mode question for SPC582B using SPC5 Studio

Hello,I'm trying to start new project which is AVAS PRJ with SPC582B. So, I'm studying it with ST EVK like below.Anyway, When I check pin mode in AutoDevKitStudio, I don't understand exaclty the meaning of pin modes(MODE_IO/MODE_GPI/MODE_OUTPUT/MODE_...

decemberdream_0-1719366541509.png decemberdream_4-1719366846659.png

Resolved! Help Needed: Undefined Reference Error in SPC5 Studio

Hi everyone, I've created a library and placed it in the directory /source/driver/. The library consists of the following files: source/driver/VN9d30Q100.hsource/driver/VN9d30Q100.c The problem I'm encountering is that when I try to use a function fr...

LuciferD_0-1718884762261.png
LuciferD by Associate II
  • 2616 Views
  • 1 replies
  • 0 kudos

Resolved! SPC560P50L3 MCU ID

Hello,The chip I am currently using is SPC560P50L3, I need a unique MCU ID for calculation, but I checked the MCU ID registers of the two chips and found that the information is the same, MIDR1=0x56042416, MIDR2=0xA8005011. is this normal?Or if there...

wybll_0-1717655092798.png wybll_1-1717655106165.png
wybll by Associate
  • 1136 Views
  • 1 replies
  • 0 kudos

Resolved! Hello! I want to ask a question about setting up EIRQ!

Hello! I would like to ask what is the meaning of setting the Latched state option in the red box as shown in the following figure? I didn't see any specific definition or explanation related to this in the SPC58 reference manual? Can you tell me whe...

QQ图片20240603110635.png
Bwang.3 by Associate III
  • 1730 Views
  • 1 replies
  • 0 kudos

Resolved! AutoDevKit Studio

Hello! I would like to ask what is the meaning of setting the Latched state option in the red box as shown in the following figure? I didn't see any specific definition or explanation related to this in the SPC58 reference manual? Can you tell me whe...

QQ图片20240603110635.png
Bwang.3 by Associate III
  • 1850 Views
  • 1 replies
  • 0 kudos

Resolved! Hello! Ask a question about the debugger!

May I use the onboard debugger on the SPC582B-DIS Discovery board to download debugging programs for the AEK-MOT-MR200G1 development board? Can you tell me which specific pins need to be connected? As shown in the following picture!

QQ图片20240527225204.png QQ图片20240527225444.png
Bwang.3 by Associate III
  • 2244 Views
  • 2 replies
  • 0 kudos

Resolved! OpenOCD common error .cfg path not found

Hi, If you are getting this kind of error when you try to run your OpenOCD in AutoDevKit Studio 2.2.1: Then most probably you have not updated the search path of the config files. From main AutoDevKit menu, select Run > Debug Configurations   In th...

MaxVIZZINI_0-1714465471083.png MaxVIZZINI_1-1714465545119.png MaxVIZZINI_2-1714465597562.png MaxVIZZINI_3-1714465679865.png