2024-05-19 11:46 PM
hi community,
I am using the "Avas Compact - Test Application" example code which is provided in the AUTODEVKIT. hear I enabled the CAN communication and it is working fine. but i want to know CAN BUSOFF is implemented or not in the given example code. if not how to implement the CAN BUSOFF.
regards
shiva
Solved! Go to Solution.
2024-05-20 1:57 AM
Hi,
>> i just want to know the "CAN BUSOFF" is implemented or not.
No, not implemented.
Best Regards,
AutoDevKit Team
2024-05-19 11:56 PM
hi,
In the original code, the CAN messages are used to increase/decrease volume and engine speed and not to start/stop the sound.
There is a button on the board to start the engine. You should implement a similar code to start the engine with a CAN message.
Best Regards,
AutoDevKit Team
2024-05-20 1:48 AM
hi
i just want to know the "CAN BUSOFF" is implemented or not.
2024-05-20 1:57 AM
Hi,
>> i just want to know the "CAN BUSOFF" is implemented or not.
No, not implemented.
Best Regards,
AutoDevKit Team
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.