Analog and audio

Find useful information on analog and audio applications: TDA7294-based designs, PDM to PCM noise, and SPICE models.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Forum board changes

Dear community member, The “Analog and audio” topic is no longer supported on the ST community. The legacy content is available only by the read-only basis. If you have any requests regarding "Analog and audio”  topics, check the alternative support ...

Resolved! Questions on the 32F746G Disco for audio DSP: How audio codec data is interpreted, compared to a typical ADC embedded inside STM32 uC.

Hi,I am currently working on developping a guitar digital looping pedal. I following my last post, I have starting looking into using the 32F746G DISCOVERY for my app, as it includes enough RAM to store audio data and has some interesting audio featu...

manurp by Associate II
  • 2192 Views
  • 2 replies
  • 0 kudos

Reducing noise on ADC input pin.

Hi guys, I am using an STM32F446RE nucleo board with an electret microphone(Waveshare Sound Sensor v2). Currently I am trying to sample audio, store it in a buffer and output through the DAC to an amplifier to a headphone jack. I am sampling the ADC ...

CReze.1 by Associate II
  • 1521 Views
  • 1 replies
  • 0 kudos

Best Low Power buffer op amp

I need to measure a signal with very low power, the signal can range anywhere between -1 and +10 Volts but i only need the 0 to 3volts for my ADC input(my battery is also 3V). is there an opamp that fits my requirements that is less than 50uA?

JWeij.1 by Associate II
  • 1513 Views
  • 1 replies
  • 0 kudos

Best practices to process and save ADC values into an SD CARD

Hello everyone,I'm trying to build a system where I could read an analog signal and save it into an SD CARD. Besides this, I need to process the signal to activate, or not, the ACC reader for a few seconds.To save the values, I decided to use two buf...

ALope.1 by Associate II
  • 1853 Views
  • 2 replies
  • 0 kudos

ADC select sampling rate

Hey guys, I am using a STM32 nucleo f446re board and I have a waveshare sound sensor v2 that I want to use. So basically just want to record audio and store it on an SD card. I want to sample audio at 44100 Hz using 8 bits, should I use a timer to ge...

CReze.1 by Associate II
  • 1348 Views
  • 1 replies
  • 0 kudos