2020-02-21 9:25 AM
Hey guys, I am using a STM32 nucleo f446re board and I have a waveshare sound sensor v2 that I want to use. So basically just want to record audio and store it on an SD card. I want to sample audio at 44100 Hz using 8 bits, should I use a timer to generate an interrupt every 1/44100 seconds to do the conversion or is there a better way to implement an exact sample rate. Thank you
2020-02-21 1:09 PM
The ADC can betriggered by a timer without using an interrupt or zthe ARM core at all. Check "Trigger ADC Conversion with a Timer" and similar discussions in the forum.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.