2024-05-24 10:47 PM
I designed a custom PCB. It is designed to be used in a remote control car I want to make/to control a BLDC motor and servo wirelessly or through a potentiometer.
When I attempt to program the microcontroller (connecting through STLINKV3) it seems to connect fine, and I am able to read the flash and option bytes. When I try to program a file, it fails with error "Error: failed to erase memory", except for one time where two blocks were written (see image) [the data is correct in the first but in the second only the 1 is correct].
I have attempted in every combination of software/hardware/core reset in CubeProgrammer, and have read various other community posts, with no success.
I'm not quite too sure where to go from here, whether it is a hardware issue or a software configuration issue.
I have attached the Altium design files as well.
Any suggestions would be appreciated.
2024-05-30 2:08 AM
Hello @nmartini,
Thank you for providing a detailed description of your issue. Could you please attach the binary file that you're trying to download and the log showing the error message you're encountering ?
Thank you in advance !
Maryem.
2024-05-30 5:10 PM
2024-06-13 7:04 AM
Hello @nmartini,
I apologize for the delay in getting back to you. Despite reviewing the files you've provided, I was unable to reproduce the issue on my end. Could you please share the current configuration of your option bytes?
Thank you for your patience and cooperation !
Maryem.
2024-06-13 5:27 PM
Hi @Maryem,
I have attached screenshots of the option bytes as I couldn't see a way to save as text. I have been unable to change any of them as well so this is how they have been configured since I received it.
Thanks,
Nick
2024-07-08 6:15 PM
Hi @Maryem ,
Have you had a chance to look at the option bytes yet?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.