STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! obDisplay API crashes

Hi,I'm trying to create a wrapper for STM32CubeProgrammer_API.dll.The program crashes on trying to use the obDisplay API. I've tried using STM32CubeProgrammer_API.dll versions 2.10 and 2.15. Is there something I'm missing?Thank you very much.

NUCLEO 64 board cannot connect to TileBox Pro

Hi  Team@ST,1. I have a Nucleo 64 board.2. I connected Nucleo64 board to TileBox Pro via SWD and [TX+RX].3. Tried using STLINK in the STM32 Cube programmer option to program TileBox Pro and i get above error message.Can you please let me know what is...

vlsireddy_0-1720635928150.png
vlsireddy by Associate II
  • 1271 Views
  • 1 replies
  • 0 kudos

STM32H7A3LIH6Q External loader

Hello.We are creating an external loader with STM32H7A3LIH6Q microcontroller and FlashROM is MX25L51245G (64MB).The development environment is as followsCubeIDE : v1.9.0CubeProgrammer: v2.13.0Microcontroller :STM32H7A3LIH6QExternal FlashROM :X25L5124...

ma-hara by Associate II
  • 1356 Views
  • 2 replies
  • 0 kudos

STM32WB10CC not programming on custom hardware

I designed a custom PCB. It is designed to be used in a remote control car I want to make/to control a BLDC motor and servo wirelessly or through a potentiometer.When I attempt to program the microcontroller (connecting through STLINKV3) it seems to ...

nmartini_0-1716614990108.png
nmartini by Associate II
  • 5162 Views
  • 5 replies
  • 0 kudos

Resolved! STM32 ST-Link Utility not working?

So i installed the st-link utility from my.st.com and did all the installation but when i run it, it tells me there are some .dll files missing. Specifically, these are the errors; 1st error; "The code execution cannot proceed because mfc140.dll was ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.