2025-02-25 7:02 AM
if we don't make a full erase, this error comes up.
I hoped it would disappear with V2.18
Solved! Go to Solution.
2025-03-03 6:23 AM
it works now with Version 2.19
2025-02-25 8:55 AM
Does it work if you upload to flash at 0x08000000?
2025-02-26 12:03 AM
with a binary file (we attached a 32bit CRC), the Programmer seems to interprete this as an offset so it must be zero.
I also tested programming it with the hex file, where 0x08000000 is selected automatically, but same error message occurs.
It only can be programmed when you first make a full chip erase.
2025-03-03 6:23 AM
it works now with Version 2.19
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.