STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32H745ZGT6 Unable to Connect

I am using the STLINK-V3SET. I have tried both the JTAG and SWD headers. 10:03:14 : UR connection mode is defined with the HWrst reset mode10:03:15 : ST-LINK SN : 00260035353251103133343010:03:15 : ST-LINK FW : V3J15M7B5S110:03:15 : Board : STLINK-V3...

IMG_5827.jpg
bmorse by Associate
  • 1462 Views
  • 2 replies
  • 0 kudos

STM32CubeProgrammer cannot connect to USBX DFU

Dear All, On my NUCLEO-U575ZI-Q I have successfully generated USBX-DFU and have come to a point to connect to it with STM32CubeProgrammer. It seems to be very simple, there are six callbacks only:USBD_DFU_Activate and USBD_DFU_Deactivate does not ret...

DmitryR by Senior
  • 1042 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeProgrammer rocky8 linux launch issue

After Install launching returns CubeProgrammer_API is missing. Please try reinstalling or check you java architecture. Ive seen some other forum posts with this issue and tried to fix the java version to no avail.Current java version is java-1.8.0-op...

re24 by Associate
  • 3812 Views
  • 7 replies
  • 2 kudos

GDPR compliance of CubeIDE and CubeProgrammer?

I just downloaded and installed both STM32CubeIDE and STM32CubeProgrammer.They both forcibly installed with user-spying phone-home features how I use the software, while only mentioning how to disable the feature after they have been installed.So, th...

SOlen.1 by Associate II
  • 6262 Views
  • 10 replies
  • 4 kudos

The only routine folder in the \bin\ExternalLoader folder in the cubemxprogrammer2.18.0 installation folder is the stldr file

我使用 H750VBTx 芯片读取寄存器0x1FF1E7FE返回值如下所示参考 https://community.st.com/t5/stm32cubeprogrammer-mcus/stm32cubeprogrammer-2-18-0-released/td-p/747840 文章,我的芯片的 bootloader 版本是否无法使用 stm32cubeprogramme2.18.0 对外部 qspi 闪存进行编程?我在哪里可以获得 \bin\ExternalLoader 文件夹中的最新可用例...

keanlee0721_0-1740065135381.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.