2022-12-28 12:46 AM
Hello,
I have NUCLEO-G031K8 and want to change nBOOT0 using STM32CubeProgrammer (v2.12.0) but I'm unable to do so.
I get four message boxes from STM32CubeProgrammer:
Even though the fourth message box says that option bytes were successfully programmed - nBOOT0 value is unchanged.
Here's log from STM32CubeProgrammer:
09:41:13 : Option byte command : -ob DUAL_BANK=1 nSWAP_BANK=1 IRHEN=1 nBOOT1=1 nBOOT_SEL=1 RAM_PARITY_CHECK=1 WWDG_SW=1 IWDG_STDBY=1 IWDG_STOP=1 IWDG_SW=1 nRST_SHDW=1 nBOOT0=1
09:41:13 : PROGRAMMING OPTION BYTES AREA ...
09:41:13 : Warning: Option Byte: DUAL_BANK, is not programmable
09:41:13 : Warning: Option Byte: DUAL_BANK, does not exist
09:41:13 : Warning: Option Byte: nSWAP_BANK, does not exist
09:41:13 : Bank : 0x00
09:41:13 : Address : 0x40022020
09:41:13 : Size : 108 Bytes
09:41:13 : Reconnecting...
09:41:14 : Reconnected !
09:41:14 : UPLOADING OPTION BYTES DATA ...
09:41:14 : Bank : 0x00
09:41:14 : Address : 0x40022020
09:41:14 : Size : 108 Bytes
09:41:14 : Bank : 0x01
09:41:14 : Address : 0x40022080
09:41:14 : Size : 4 Bytes
09:41:14 : OPTION BYTE PROGRAMMING VERIFICATION:
09:41:14 : Option Bytes successfully programmed
09:41:14 : Time elapsed during option Bytes configuration: 00:00:01.199What's strange I can change nBOOT0 using old, depreciated STM32 ST-LINK Utility (v.4.6.0).
Does anyone have a clue what I'm doing wrong?
Thanks!
Solved! Go to Solution.
2022-12-30 12:02 AM
Hello @Community member,
Thank you for posting,
You are doing nothing wrong, this is a bug in the latest release of STM32CubeProgrammer and is internally reported.
Internal ticket number: 139785 (This is an internal tracking number and is not accessible or usable by customers)
I apologize for the inconvenience. While programming your STM32G031 option bytes, I suggest using CLI or STM32CubeProgrammer v2.11.0.
Aziz
2022-12-30 12:02 AM
Hello @Community member,
Thank you for posting,
You are doing nothing wrong, this is a bug in the latest release of STM32CubeProgrammer and is internally reported.
Internal ticket number: 139785 (This is an internal tracking number and is not accessible or usable by customers)
I apologize for the inconvenience. While programming your STM32G031 option bytes, I suggest using CLI or STM32CubeProgrammer v2.11.0.
Aziz
2022-12-30 1:07 AM
Hi @Community member ,
As said by @Aziz BRIGUI this issue is already raised and will be fixed in next CubeProgrammer release.
Meanwhile you can use the CLI, it works fine or 2.11.0 version.
Hope this helps you.
Houda
2022-12-30 1:58 AM
@Aziz BRIGUI @Houda GHABRI - thank you for quick and solid answer, I tried previous STM32CubeProgrammer version (v2.11.0) and everything works as expected :)
PS Is there any document in public which lists/describes known bugs in STM32CubeProgrammer?
2022-12-30 2:28 AM
For known limitations, you can check the release notes for STM32CubeProgrammer available under this link. However since this bug is new, you won't be able to find it in that document.
I hope this helps,
Aziz
2022-12-30 2:52 AM
Thank you - that's exactly what I was looking for :)
2023-03-03 12:19 AM
Hello @Community member,
Issue is resolved in latest STM32CubeProgrammer version (v2.13.0) available under this link.
Aziz
2023-03-09 4:17 AM
Thanks :) I'll check that out.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.