cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 IAP bootliader does not work with user application >50kb

JBond.1
Senior II

Hi, I have STM32F407VET6 with a bootloader which reads microSD card, checks for user application update, flashes if it exist and jumps to use application 0x08004000.

All was working fine when my user application was <48kb. I wrote some additional code (which should not impact the start of the application), and now id does not work.

Previously debbugging started at "HAL_Init()" like it should when user application was <48kb

0693W00000DmsMdQAJ.png 

But now, when user application is >50kb it starts debugging at some kind of wrong address:

0693W00000DmsNMQAZ.png It does not hit "HAL_Init()" anymore like it should.

Why user application size could impact that? Or it could be some kind of different issue?

How could I fix this?

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12

I always set heap to 0 since I dont use it, but seems that dynamic arrays need it.

Constructors don't use heap space unless you're dynamically allocating them with new/malloc or things within them, which would be an odd choice if they're globally defined.

Can't see why the posted code would need heap. I compiled it with GCC and it's using the stack there.

When you debug, you can start at Reset_Handler, which is the very first thing executed after reset. If it winds up in HAL_Init, some code is causing it to move there. main() is eventually called, but that's not where it starts. In CudeIDE, there is a startup_*.s file. I imagine there is something similar in Keil.

If you feel a post has answered your question, please click "Accept as Solution".

In the 1st case you use the C99 feature: allocation of variable size array (VLA) on stack.

Probably the compiler or runtime library does not quite support this.