STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32G0 don't start and connect after update

Dear,I have a big problem on a STM32G070 and I don't know what I can do to solve it.The system is composed of 2 boards with a STM32G0B1 for the first (master board) and a STM32G070 for the second (slave board).The 2 MCUs are connected by UART and thi...

YDann.7 by Associate III
  • 7671 Views
  • 12 replies
  • 0 kudos

Debug issue

Hello, I have an issue debug issue in my custom board. The debug session works for a while and then stop to working and suddenly after many tries it works again. When the debug session doesn't work, I get:STMicroelectronics ST-LINK GDB server. Versio...

NASI by Senior
  • 9788 Views
  • 12 replies
  • 0 kudos

STL Library CRC Calculating

I am using the STL library from X-CUBE-STL. To check the data in flash, I have to calculate CRC in the post build section and upload it to flash. ST provides an example post build command for this. But there is a problem, no data in flash is filled w...

How to include the CubeProgrammer_API.dll file in C application to access the API's of STM32CubeProgrammer?

Hi Team,I am working on one of the Project where I have to update the new firmware over the UART using System bootloader without STM32CubeProgrammer tool.So, for this I need to implement the C application using STM32CubeProgrammer API's.Therefore, I ...

AMull.11 by Associate II
  • 2255 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.