2025-07-07 10:06 AM
Hi,
I'm using STM32CubeIDE with an ST-LINK V2 debugger (possibly a clone). When I try to upload my program to the STM32 board, I encounter the following issues:
1. ST-LINK not entering DFU mode, so I can't update firmware.
2. STM32CubeIDE gives this error:
Error with command: GNU debugger version --version
Cannot run program GNU debugger versi: Launching failed
Setup:
- STM32CubeIDE 1.18.1
- ST-LINK V2
- Board: STM32F103C8T6
- Windows 10
Things I tried:
- Installed ST-LINK drivers (STSW-LINK009)
- Installed STM32CubeProgrammer
- Checked Device Manager: ST-LINK appears
- Tried STM32CubeIDE reinstall
Need help with:
- Forcing DFU mode for ST-LINK V2
- Resolving GNU debugger version - issue in STM32CubeIDE
Thanks!
2025-07-07 10:22 AM
@mariam-varkey1234 wrote:an ST-LINK V2 debugger (possibly a clone). !
How to check for sure:
TL;DR:
@mariam-varkey1234 wrote:- Board: STM32F103C8T6
That's just a chip part number - it doesn't identify a board.
Are you sure the chip isn't (also) a clone/fake?
@mariam-varkey1234 wrote:- Installed STM32CubeProgrammer
And were you able to do anything via CubeProgrammer?
2025-07-07 6:56 PM
STM32CubeIDE doesn't work well with non-genuine chips or programmers.
> Forcing DFU mode for ST-LINK V2
This doesn't make sense. DFU is a USB-peripheral that lets you update firmware over USB without a programmer. If you're using an ST-Link, it's not involved here. Are you connecting over SWD?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.