2025-05-19 5:23 AM
Hello,
I am currently trying to program a nucleo board using USART. For this I am using the bootloader and Cube Programmer.
I first developed a program and tester it by programming via st link. My program worked with no problem. I then tried to program using UART.
I was able to connect but as soon as I started programming, I get the message Error :GETID command not acknowledged and then the nucleoboard is disconnected.
Here are my settings and the boot0 pin is tied to 3.3V.
When I program I can see on the oscilloscope that some part of the program is on and working but not fully as well.
Any idea ?
Thanks very much
Solved! Go to Solution.
2025-05-23 6:17 AM
Thanks for helping !
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.