2023-03-17 10:07 AM
My Settings :
STM32G070 mit BootLoader protocol version: 3.1
STM32CubeProgrammer v2.13.0
My plan :
flash my file via UART(USART2) and my MCU should start automatically after programming is finished. I will reset the nBOOT0 bit in my programm, after my own evaluation.
My result :
I tried with "Run after programming" in CubeProgrammer and "Go 0x800000" in STM32_Programmer_CLI. In both case, downloading was successfull but MCU could not start.
See attached log file : logCP_uart.log
Step 1 : nBOOT0 = 0, nBOOT1 = 1, nBOOT_SEL = 1 : this combination by Stm32G070 leads to boot from System memory (Bootloader)
Step 2 : I could access boot loader via uart (com16) and start programming.
Step 3 : My Transmitter.elf file was downloaded (line 32) and the Verifying was also successfully (line 36).
Step 4 : But the RUNNING Program from Address 0x08000000 (line 37 and 38) could not be executed. Error Message : Error: GETID command not acknowledged! (line 44)
See attached log file : logCP_CLI.txt
Log file says, that RUNNING Program was a success. But my MCU has not started.
See attached log file : logCP_swd.log
Test to compare:
I chose SWD instead of UART. In this case, the task could be executed without any problem.
Solved! Go to Solution.
2023-03-17 10:15 AM
Some STM32 need power cycling after programming
Check if the watch-dog is running, you're code may run, but you'll still have to kick it.
Has it really not started? Toggle GPIO very early in Reset_Handler
2023-03-17 10:15 AM
Some STM32 need power cycling after programming
Check if the watch-dog is running, you're code may run, but you'll still have to kick it.
Has it really not started? Toggle GPIO very early in Reset_Handler
2023-03-17 10:56 AM
A Great Thank for Your speedy help.
I've tried with toggling GPIO before the main starts.
Yes, my MCU has toggeled !
Now I have found out, one of our function has blockt the init process, which we have packed in startup_stm32xxx.s file. I must figure out, why this makes problem.
But my problem i have posted is solved!!!
Thanks a lot for your help!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.