2018-03-02 12:49 PM
I'm trying to use the dual bank feature in the Nucleo-l152re dev board. I want to understand how I can use program bank 2 (address 0x08040000) using the STM32Cube Programmer using the onboard USATR1.
I understand that I need to enter the boot mode using the BOOT0 pin, connect after system reset and flash by programming the appropriate image file. The problem is :
-- I cannot find the option to choose the bank
-- the option to put in the start address is not highlighted.
Although i can choose the value of option byte: checked for 0 or unchecked for 1, no point loading from bank 2 when there is nothing on there.
Any help will be appreciated.
#stm32cube-programmer #nucleo-l152reWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.