2025-11-03 5:08 AM
Hey there,
Is there an option to turn off the prompts after programming in the STM32CubeProgrammer?
The Log output is enough for me:
Not really a problem, more like a QoL thingy - but i didn't see an option anywhere.
Would be a nice addition if it's currently not present. Like "only prompt on errors"
Solved! Go to Solution.
2025-11-04 5:23 AM
Hello @Proxi,
This request is already tracked internally (Internal tracking number: 195238).
In the meantime, you can use the CLI to work around needing to close the pop-ups. Will make sure to give you the update when this is implemented.
Aziz
2025-11-04 5:23 AM
Hello @Proxi,
This request is already tracked internally (Internal tracking number: 195238).
In the meantime, you can use the CLI to work around needing to close the pop-ups. Will make sure to give you the update when this is implemented.
Aziz
2025-11-04 5:26 AM
Great, thanks for letting me know!
That would be much appreciated!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.