2023-11-17 7:31 AM - last edited on 2023-11-20 5:53 AM by KDJEM.1
Hello,
I'm trying to setup a production line where I have to flash a serial number on each piece after it has been programmed with the standard firmware.
I put the serial number in an hex file, and I'm trying to write it using STM32_Programmer_CLI but I need to skip the flash erase before programming.
I tried using 'ske':
STM32_Programmer_CLI.exe -c port=SWD -w serial.hex ske
but the flash keeps getting erased.
I found out that with ST-LINK_CLI.exe I can use the option 'ske' to disable flash erase, and I tried it, but it seems kind of obsolete because when I launch
ST-LINK_CLI.exe -c SWD LPM -P serial.hex ske
I keep receiving this error:
Note that read out protection is NOT enabled and there is no elf file involved, I'm using .hex files.
What am i missing here? From what I can understand SMT32 Cube Programmer should have replaced STLink Utilities, but is it missing fundamental features like skipping the erase of the flash?
Solved! Go to Solution.
2023-11-17 8:48 AM
I found out this question
where they use
STM32_Programmer_CLI -c port=USB1 -d myHex.hex --skipErase
I tried "--skipErase" with STM32_Programmer_CLI and it finally works!
The thing is, I cannot find this info in the STM32CubeProgrammer User manual, even if there's a chapter focused on command line programming.
My advice for ST would be to work a bit on the documentation of STM32 Programmer, because I had to find my solution on the answer to a question about a totally unrelated topic!
2023-11-17 8:48 AM
I found out this question
where they use
STM32_Programmer_CLI -c port=USB1 -d myHex.hex --skipErase
I tried "--skipErase" with STM32_Programmer_CLI and it finally works!
The thing is, I cannot find this info in the STM32CubeProgrammer User manual, even if there's a chapter focused on command line programming.
My advice for ST would be to work a bit on the documentation of STM32 Programmer, because I had to find my solution on the answer to a question about a totally unrelated topic!
2023-11-17 9:51 AM
2023-11-20 4:59 AM
Hello,
Thank you @ElPueblo and @Pavel A. for bringing this issue to our attention.
I reported this request internally.
Internal ticket number: 166662 (This is an internal tracking number and is not accessible or usable by customers).
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-25 2:59 AM
Hello @ElPueblo and @Pavel A. ,
The SkipErase command is currently described in UM2237 Rev 24.
Thank you for your contribution in STCommunity.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.