2023-10-02 2:43 AM
Using STM32_Programmer_CLI.exe (v2.13.0, on Win10) I try to connect via ST-Link / SWD, It works perfectly in the GUI but if I try
STM32_Programmer_CLI --connect port=SWD ap=1
nothing happens, not even an error, it just terminates. I can even write nonsense after the --connect - no response.
--list works fine:
-------------------------------------------------------------------
STM32CubeProgrammer v2.13.0
-------------------------------------------------------------------
===== DFU Interface =====
No STM32 device in DFU mode connected
===== STLink Interface =====
-------- Connected ST-LINK Probes List --------
ST-Link Probe 0 :
ST-LINK SN : 003E00303331511134333834
ST-LINK FW : V3J11M3B5S
Access Port Number : 1
Board Name : STLINK-V3SET
-----------------------------------------------
===== UART Interface =====
Total number of serial ports available: 1
Port: COM6
Location: \\.\COM6
Description: STMicroelectronics STLink Virtual COM Port
Manufacturer: STMicroelectronics
What am I missing here? Thanks!
Solved! Go to Solution.
2023-10-02 3:28 AM
If found a work around, maybe someone else is interested:
On my workstation there is also the CubeIDE installed, which brings its own STM32_Programmer_CLI.exe. For the failed attempts I tried to use the CLI-exe from the "normal" windows program folder, where also the GUI version is located. In my case C:\"Program Files"\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe
Now I switched to the IDE-version at C:\ST\STM32CubeIDE_1.12.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.0.600.202301161003\tools\bin\STM32_Programmer_CLI.exe and it works as expected. Maybe dll-hell deep inside, I won't investigate further.
2023-10-02 3:28 AM
If found a work around, maybe someone else is interested:
On my workstation there is also the CubeIDE installed, which brings its own STM32_Programmer_CLI.exe. For the failed attempts I tried to use the CLI-exe from the "normal" windows program folder, where also the GUI version is located. In my case C:\"Program Files"\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe
Now I switched to the IDE-version at C:\ST\STM32CubeIDE_1.12.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.0.600.202301161003\tools\bin\STM32_Programmer_CLI.exe and it works as expected. Maybe dll-hell deep inside, I won't investigate further.
2024-01-29 7:37 PM
Did you try shared mode of two ST tools?
https://wiki.st.com/stm32mcu/wiki/STM32CubeMonitor:How_to_configure_shared_mode
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.