STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

ST-Link v2 Cube programmer

Hi all, new to this. I am trying to remove read and write protection. In the option bytes, I cannot change wrp-0 and wrp-1. The progress bar on the lower part of the gui says 100% but does not actually finish. when I check the live update box, I get ...

LesterC by Associate
  • 1410 Views
  • 2 replies
  • 0 kudos

Resolved! Why might setting BFB2 cause printf to stop working?

I've written a fairly simple test case for using the system bootloader to boot from flash bank 2 on a STM32F429ZIT6U (developing on a Nucleo F429ZI board). With stdio redirected to a UART, I'm able to direct the code to:Mass-Erase Bank 2Copy the ent...

Brian H by Senior
  • 8737 Views
  • 14 replies
  • 0 kudos

Programmer CLI - safety lib - <pattern> parameter

We are using the safety lib (-sl) command with X-CUBE-STL library. Without <pattern> parameter, it is working. When trying to use 0xFF for <pattern> parameter, generated .elf is not even valid and cannot be loaded. Is there a workaround for this?For ...

Program loading is failed

Hey Team, I am working on STM32H745 for display project.I have faced following issue. Some time when I was program my device it was completed in 1.38 minutes usually it takes around 4 minutes because of external flash erase and program loading. 1) Is...

APate.18 by Associate III
  • 2419 Views
  • 5 replies
  • 0 kudos

Resolved! ST-link V2 Connection error.

How do I solve this error? "Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication"I use SWD. I made the cable for SWD communication. The cable is connecting ST-LINK V2 between...

KimJeBu by Associate II
  • 31492 Views
  • 24 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.