STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! STM32CubeProgrammer External Loader Partial Page

Hello, I have made a custom external flash loader(.stldr) file for my STM32 based board. Reading the content of the external flash via CubeProgrammer works fine. But when programming i run into the following problem: CubeProgrammer tries to write par...

CRich.4 by Associate III
  • 5386 Views
  • 10 replies
  • 2 kudos

Resolved! X-NUCLEO-LPM01A board not found on Windows 10 or MAC

i've installed versions of STM32CubeProgrammer on my windows 10 PC as well as my MAC....i'm following the instructions in um2269 (section 8) on updating firmware, but see a message saying "No DFU detected" under the USB configuration panel....  selec...

biosbob by Associate
  • 1756 Views
  • 1 replies
  • 0 kudos

STM32 cube programmer

Hello everyone,I am trying to connect device with stm32  cube programmer vai UART connection I am not able to connect initial but as some resource form st community and other online article I able to connect but it not able get into application is th...

PESHWA by Associate II
  • 2945 Views
  • 6 replies
  • 0 kudos

API: STLink detected but cannot be connected to.

I want to use the STM32CubeProgrammer C++ API to do high-speed real-time automated debugging (i.e. use it as an oscilloscope). I used as a basis the Example_2 given in the API's documentation. The STLink is detected since I can get info from it which...

_legacyfs_online_stmicro_images_0693W00000bjDGPQA2.png
AMabi.1 by Associate III
  • 4033 Views
  • 7 replies
  • 1 kudos

cube programmer - leave dfu

hi in the previous tool DFude v3.0.6 we had a button called -leave dfu mode,that button made disconnection and reset to MCU if you were connected with USB, so after flashing the MCU jump to application FW,now in the cube programmer, we don't have thi...

NBita.1 by Associate II
  • 2123 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.